Issue
Looking for actuator with position feedback signal for V321 (V292, V222) DN125-DN150 since M22/M50 does not provide this option.
Environment
- V222 DN125
- V222DN150
- V292 DN125
- V292 DN150
- V321 DN125
- V321 DN150
- M22
- M50
Cause
Actuator with positioning feedback signal for DN125 - DN150 valves
Resolution
There are currently no suitable actuators available that gives the Forta features on the M22/M50 actuators. Also, there is no linkage kit that would make the Forta series actuators fit on the DN125 and DN150 size valves, due to its different design.