Satchwell Climatronic Controller displays TEST on Liquid Crystal Display screen.

Issue

The word TEST is displayed on the Liquid Crystal Display screen of a Satchwell Climatronic Controller when first powered up during initial installation preventing it from being commissioned.

Product Line

Field Devices

Environment

  • Satchwell Climatronic
  • CSC5252
  • CSC5352
  • CXR5805
  • CXT5605
  • CZT5305 
  • Controller Display
  • TEST
  • LCD Screen

Cause

The cause of the word TEST being displayed on the Liquid Crystal Display screen of a Satchwell Climatronic Controller when first powered up during initial installation and preventing it from being commissioned is normally due to a micro processor programming error occurring during the course of production.

Resolution

There is no field remedy that can be applied to a Climatronic Controller displaying the word TEST on the Liquid Crystal Display screen that will enable it to be commissioned successfully.

The Controller should therefore be returned to the vendor for replacement under the terms and conditions of the warranty applicable at the time of purchase.