Issue
Defining flow direction in VZ308 valve.
Environment
VZ308
Cause
Flow direction definition in mixing application.
Resolution
As described in the data sheet:
The valves should be installed as mixing valves,
with ports connected as:
Port AB: Combined flow outlet
Port A: Controlled flow inlet
Port B: Bypass inlet