Issue
While trying to create a point mirroring program with multiple lines. Several (but not all) lines with references to remote Infinet points indicate the above error.
Environment
CyberStation v1.93
Plain English IDE
Net2 with Infinet2's
Cause
The following error occurs on several lines of a program being saved:
"The specified directory service attribute or value does not exist"
Resolution
- Reload the remote controllers (the Infinet controllers with the points creating the errors in the PE program)
- Delete the mirroring point program in the Net2.
- Reload the Net2.
- Recreate the program in the Net2 and save successfully.