SE7200 handling simultaneous applications

Issue

Want to be able to run the SE7200 in floor heating and chilled beam simultaneously.

Product Line

Field Devices, SmartStruxure Lite

Environment

SE7200

Cause

running simultaneous applications.

Resolution

Unfortunately the SE7200 will only handle 1 main application per controller due to its limited I/O.