Issue
How can you determine what standard drivers are included with the basic I/A Series G3 hardware product license?
Environment
I/A Series G3 (Niagara) hardware License (ENS, ENC, NXT, etc.)
Cause
Product data sheet is not clear in regards to what license options are included with the standard basic license for an I/A Series G3 hardware products.
Resolution
Refer to the TAC I/A Series G3 Hardware License Request form.
In the "I/A Series G3 Drivers" section of the form there is a box that contains text beginning with "Standard drivers for the xxx include". This box lists the complete set of standard drivers included with the license for associated hardware product.
For example, at the time this is written, the ENC-520 Series TAC I/A Series G3 Hardware License Request form shows the following:
This box indicates that the following drivers are included with the standard license for an ENC-520.
- LON
- BACnet-IP / BACnet-Ethernet (Client only)
- BACnet MS/TP
- oBix Client / Server
The ENS-1, ENC-410 and JACE-NXT have similar lists of included drivers. Refer to the license request form for the hardware product for the list of included drivers.