Issue
Does not want to create his application from scratch if there are application templates available.
Environment
MNL series of standard LON controllers (MNL-50, 100, 110, 130, 150, 200, V1R, V2R, V3R series).
Cause
Wants to start with a pre-engineered application if one is available.
Resolution
- Download WPT Micronet Applications Library v4.0.zip.
- Extract the files to the Solutions folder in WPT.