Issue
Is it possible to save a report as a CSV file from Vista?
Environment
Vista 5.1.X
Cause
This is a limitation of the software. It is only capable of saving the default file type of XLM.
Resolution
It is only possible to save a report as XLM not CSV. To create a CSV, open the report in the Excel format (XLM) and then perform a manual "Save As" function to select the CSV extension for the resulting file.