Issue
Added the MSTP Status object to the MNB-1000 database and connected a constant tag to its network input and tested it with WorkPlace Tech and it functions as expected. However, when doing a Device Learn of this MNB-1000 at the UNC it fails.
The messages is "Learn Device Failed. ObjectId [binary_value:589834]". The instance number after the binary_value may be different depending on other status objects in the database.
Environment
I/A Series Niagara R2
Cause
Cause is being investigated.
Resolution
Use the Device Status object instead. It will perform the same function and can be learned at the UNC without issue.