Can not get CIPCL to autostart

Issue

Can not get CIPCL to autostart

Product Line

TAC Vista

Environment

  • TAC Vista
  • Windows 2008 R2
  • Windows 7

Cause

Windows will not allow modification of the registry unless the application is started with the "Run as Administrator" option.

Resolution

Right click on TAC Vista Server and choose Run as Administrator.