Issue
Getting warning " Received bit string (25) is longer than expected length (23)" in the standard output window. Is this a problem?
Environment
I/A Series R2 G3 BACnet Niagara
Cause
This warning is because the UNC was reading the list of object types supported from the device, and the device was implemented to a different protocol revision, in which there were a different number of object types defined.
Resolution
The UNC ignores this, and it has no negative impact.