RPC Error Troubleshooting on Cyberstation

Issue

There are a number of reasons that RPC error occur on Cyberstation and troubleshooting steps are needed

Product Line

Andover Continuum

Environment

Continuum

Webclient

Windows XP

Window Vista

Windows 7

Windows Server 2003

Windows Server 2008

Cause

RPC (Remote Procedure Call) errors happen on Cyberstation when the connection to the SQL database is not available

Resolution

There are many reasons that RPC errors can occur. A Google search of RPC errors will indicate that many applications have similar issues with these errors. The document below can be downloaded in order to help troubleshoot RPC errors when they are happening on Cyberstation. Other steps will be added to this documents as we continue discover additional reasons why this happens.

Click here to download Cyberstation RPC Error Troubleshooting

* Update to 1.94 SP1