Is there a I/A Series R2 tunnel client available that will run on any Windows 7 computer?

Issue

Is there a I/A Series R2 tunnel client available that will run on any Windows 7 computer?   The existing I/A Series Tunnel clients cannot be used on Windows 7 64-bit and some issues occur when used on Windows 7 32-bit.

Product Line

TAC I/A Series

Environment

I/A Series R2 UNC

requirements for Serial, ASD, MicroSmart or LON tunneling through that UNC.

Cause

Existing I/A Series R2 Tunnel Clients were not developed for use on Windows 7

Resolution

The AxTunnelClients can now be used with the I/A Series R2 UNCs. The new I/A Series R2 jar files required are on The Exchange Download Center. For details see the release notes in the tunnelAx zip file.

As noted in the release notes, new jar files have also been released to allow the use of the AxTunnel client for ibsASD and ibsMS serial tunneling. Those jar files are also in the same 532 files area.