Field Devices - IAC Touchscreen passwords.

Issue

IAC Touchscreen passwords.

Product Line

Field Devices

Environment

IAC

Touchscreen

600

IAC600

Cause

Customer did not know the passwords.

Resolution

The password that will allow you to read point values via the Touchscreen is 1234.

The password that will allow you to make changes to point values via the Touchscreen is 4321.

There is also a maintenance password available, but unless the operator knows the Touchscreen operation well, this should not be used. Please refer to Product Support Services if this password is required.

To view the Touchscreen User Guide, please click HERE.