Lost license file Vista IV

Issue

If the license file (.plf) is lost, it is necessary to recover it for reinstall.

Product Line

TAC Vista

Environment

TAC Vista versions from version 3.30 to 4.50

Cause

The license file is necessary for the system to run. In case of crashed PC or similar, the license file needs to be reinstalled together with its matching dongle.

Resolution

As long as the dongle ID or Order no. can be presented, it may be possible to regenerate the .plf license file.

Please contact the Product Support Services for further assistance.

Official support of Vista IV licensing has been suspended as of 1/1/2012.