Issue
Is there a document that gives the suggested controller to I/O device (field hardware) wiring information? Wire Gauge, Type of Wire, etc.
Environment
I/A Series controllers and field hardware
Cause
Customer wants a document that provides Schneider-Electric's recommendation on controller field wiring.
Resolution
For the MNB family of controllers, refer to the MicroNet BACnet Wiring, Networking and Best Practices Guide, F-27360.
For the MNL family of controllers, refer to the I/A Series MicroNet System Engineering Guide, F-26507.
For the Network-8000 family of controllers, refer to the Network 8000 Hardware Installation Practices guide, F-23061.
The Network 8000 Hardware Installation Practices guide is also a good guide for field device wiring for use with any family of controllers.