Field Devices - Drayton DC 2000/2100 and 3000 controller series.

Issue

Drayton DC 2000/2100 and 3000 controller series.

Product Line

Field Devices

Environment

Drayton

DC

2000

2100

3000

Cause

Are replacements available for the Drayton DC 2000/2100 and 3000 controller series?

Resolution

The Drayton DC 2000/2100 and 3000 controller series are obsolete, and there are no direct replacements for these controllers.