There is no way to view the personnel records stored in a NetController

Issue

Is there a way to see what personnel objects are in the Netcontroller?

Also, there is no way to send the personnel records (or area objects) from the controller into the SQL DB.

Doing a 'Send to database' will NOT send personnel records or area objects.

Product Line

Andover Continuum

Environment

All Access Controllers

Cause

Viewing personnel records

Resolution

There is no way to view the personnel records stored in a NetController.