Field Devices - Replacement for a V295 steam valve and an M750 actuator.

Issue

Replacement for a V295 steam valve and an M750 actuator.

Product Line

Field Devices

Environment

V295

Steam Valve

M750

Actuator

Cause

Unable to purchase a V295 steam valve and an M750 actuator.

Resolution

The V295 steam valve and an M750 actuator are obsolete.

M750 - 24v - 880-0010-000 -  Not available -

To operate on steam you will require a spring return actuator, the M700-SRSU (880-0430-000).

V295 - DN 40, PN25, KVS25 - Not available.

A replacement could be the VGS211F-40CS please note this valve has a rating of PN16, where as the V295 was PN25.

To review the VGS211F data sheet, please click HERE.

To review the M700 data sheet, please click HERE.