Issue
DC1100 / DC1400 Optimiser / Compensator Controller Holiday Date amendment / removal.
Environment
- DC1100
- DC1400
- Optimiser Compensator Controller
Cause
Amendment / removal of DC1100 / DC1400 Optimiser / Compensator Controller Holiday Date required.
Resolution
- Select SET on Front Panel Switch
- Select HOLIDAY DATES from menu options
- Select SET HOLIDAYS
- Select SET HOLIDAY START & STOP DATES
If start-stop dates are selected as being the same, then Holiday Date or period is ignored.
Details appear in the DC1100 Installation document which may be viewed here.
Details appear in the DC1400 Installation document which may be viewed here.