Issue
Attempting to view I/A Series G3 graphics via browser. Error indicates HTTP 501 "Not Implemented" error with the message "Module content filter excludes user interface packages."
Environment
I/A Series G3, ENC-410, ENC-520
Cause
When an ENC is accessed from a browser, it is necessary that the user interface packages be available to correctly render the web-based display. When these packages have been filtered out, the browser will report an HTTP 501 "Not Implemented" error with the message "Module content filter excludes user interface packages."
Resolution
To correct the module content filter must be changed to include the UI package and the associated modules must be re-installed.
- Open the platform for the ENC and run the Commissioning Wizard.
- Clear all selections and enable "Select module content filter level."
- Step through the commissioning process and change the Module Content Filter Level to UI+RUNTIME.
- Continue through the commissioning process and Finish to install the UI modules.