Issue
A Niagara R2 station is being upgraded from version 431 to 529. A copy of the station from 431 is successfully converted to xml. However, the config.xml does not convert to a config.db or a config.sns in version 529.
The following error appears in the conversion window:
------- Errors -------
ERROR: c:\niagara\r2.301.529\stations\Blake\config.xml(630110,66):
Could not parse value.
Invalid dateTime "60356-06-20T10:54:24.17-7".
Parse of XML failed.
----- End of input -----
Environment
Niagara R2 all versions
Cause
Somehow, an incorrect date reference was registered in the station. It may have occurred during the creation of the config.xml.
Resolution
Using a XML editor utility (ie: Notepad++), modify the date so that it reads "2011" instead of "60356".
from: <lastDailyArchive>60356-06-20T10:54:24.17-7</lastDailyArchive>
to: <lastDailyArchive>2011-06-20T10:54:24.17-7</lastDailyArchive>
Run a conversion again.