Issue
When do I need the -U (unlimited I/O) option enabled on my Continuum Security Key?
Environment
Continuum Cyberstation
Cause
Ordering new Continuum Security Key for existing site. Unsure if -U option is require if specific Workstation is only going to be viewing less than the 1000 I/O limit, even though there are more than 1000 I/O on this entire site.
Resolution
If your site has more than 1000 combined inputs and outputs then you will need to use the unlimited (-U) option for the Continuum Security Key to be able to see all I/O. Without the -U option, the Workstation will be limited to the first 1000 input and output points.
You are unable to pick and choose which 1000 points you wish to see at each workstation, if your site has more than that defined then you will need to order the -U option on your Continuum Security Key.