I/NET Software - Part Numbers and License Rules

Issue

  • Need to confirm the correct part number to upgrade I/NET
  • Do I need to pay for the I/NET software to upgrade the site?
  • When can I use a SEAT license?
  • What are the rules / definitions for using SEAT / SITE Licenses with I/NET?

Product Line

TAC I/NET

Environment

I/NET Software

  • I/NET 2000
  • I/NET Seven to 2.4x

Cause

Confusion with part numbers and license restrictions within I/NET software offering. 

Resolution

 Ordering information is usually contained within each of I/NET's Product Announcements. These are found on The Exchange Download Center as well as on Article #4240.

When upgrading from a “minor” revision, upgrades from v2.40 are free. All you need is the new version of v2.4x software which can be downloaded at no charge from the Buildings Business Extranet website.

To download TAC I/NET Seven software, refer to Article #6163

Upgrades from pre-2.4x versions (i.e. v2.3x and below) are paid upgrades. Standard upgrade prices are the same whether upgrading from I/NET Seven v2.31 or I/NET 2000. When upgrading, all host PCs must be upgraded to the same version.  Upgrade / New Ordering part number information can be found in Article #7124

For information that needs to be provided during the ordering process or if you have an issue with the Site License key refer to Article #3997


I/NET Seven Software Definitions

Site Licenses

  • SEVENHVAC
  • SEVENMAX
  • SEVENSEC

Definition of a SITE:

“A building or collection of buildings at single or multiple locations owned and operated by ONE end user, upon which I/NET is installed.”

Seat License:

  • SEVENSEAT

Definition of a SEAT

“A license for an additional PC at a SITE as defined above, irrespective of configuration i.e. Remote Client, Filemaster, Equalized Client etc.”