Sigma - The Analogue output card only produces 9.9 volts dc.

Issue

The Analogue output card only produces 9.9 volts dc.

Product Line

Satchwell Sigma

Environment

Sigma

Analogue Output

Voltage

Cause

The Analogue output card only produces 9.9 volts dc, can it produce 10 volts?

Resolution

No, although the card is said to produce 0 - 10 volts, it will produce slightly less.

For the data sheet please click here.