Sigma - Programme to provide a 48 hour average value.

Issue

Programme to provide a 48 hour average value.

Product Line

Satchwell Sigma

Environment

Sigma

Programme

Program

Average

48 hour

Cause

The customer requires a programme that will record the outside temperature every hour, on a rolling 48 hour basis.

Resolution

This programme has been produced to operate in a UNC632 controller, but can be modified if required to operate in an X96.

If modified, it is important to keep the sequence of objects in the same order as at present.

This programme was created at Sigma 4.05 SEB (build 3.42.18).

Please click HERE to download the programme files.