Webpinpoint will not run Plain English script that works in Cyberstation Pinpoint

Issue

Nothing happens or an error ' You have insufficient rights to perform this operation' happens when clicking a webpinpoint graphic that is set up with a Plain English script.

Product Line

Andover Continuum

Environment

Webclient

Web Pinpoint

Windows XP

Windows Vista

Windows 7

Windows Server 2003

Windows Server 2008

Cause

Webpinpoint does not support running PE programs like Cyberstation Pinpoint does.

Resolution

Webpinpoint does not support running PE programs like Cyberstation does.

A possible work around to this would be to set up a numeric that gets changed when a button is pushed.

A program can be set up as looping to be triggered by this numeric and the code executed to perform the operation needed.