'Unable to request license' message when using Demo license with Remote Workstation.

Issue

'Unable to request license' message when using Demo license with Remote Workstation.

Product Line

TAC Vista

Environment

Vista 5

Vista 4

Cause

The Demo license only works when installed on the same PC as Vista Server.

Resolution

Install demo license on the Vista Server PC and run Workstation on the same PC.  If remote Workstation operation is required or the license server is on a different PC to Vista Server, purchase an end user license.