Issue
Is it necessary to commission an MNB series controller if it is being used in a standalone application?
Environment
Single standalone MNB series controller
Cause
Using an MNB-300 controller to control a small RTU via an attached MN-sx sensor during construction.
Resolution
No.
Commissioning is needed only when the device is being configured to communicate via its BACnet interface.