Alarms in standalone programmable Xenta

Issue

  • How many alarms are stored in a standalone Xenta?
  • What happens with alarms in a programmable Xenta if no Vista is connected?

Product Line

TAC Vista

Environment

TAC Xenta 301, 302, 401, 281, 282, 283

Cause

There is a limit on how many alarms a Xenta can store before the memory gets full.

Resolution

The TAC Xenta will store up to 20 alarms after that it is "First in first out", meaning that when the 21st alarms comes in the oldest alarm will be overwritten.