Issue
Browser locking up with blank screen after viewing several graphics. Java console says java.lang.OutOfMemoryError: PermGen space.
Environment
IA Series Niagara G3
Cause
This can occur when viewing graphics screens from different ENC stations that have differing versions of modules. The browser will load the modules it needs from each ENC which can eventually use up all the available PermGen memory.
Resolution
Make certain all ENC stations are using the same version of the modules needed.