Issue
Method for increasing the security of Vista Webstation.
Environment
Vista Webstation 5.1.7
Internet Information Server (IIS)
Internet Security and Acceleration Server (ISA)
Cause
Increased Webstation security is limited by the security of Internet Information Server (IIS). Webstation is only a web application running on the IIS, therefore to make webstation more secure is to make the connections to the IIS more secure.
Resolution
Security can be increased by using an Internet Security and Acceleration Server (ISA). The IIS would then reside on a computer behind the ISA server.