Issue
Installing I/NET on a Virtual PC and how to get it to work properly.
Environment
- All versions of I/NET
- Server 2008R2 (64bit)
- Server 2003
- Windows 10 64bit (Inet 2.49 only)
- Windows 8
- Windows 7
- Windows XP
- SQL versions 2005, 2008
- VMWare
Cause
This is an unsupported application as I/NET was not tested in this environment due to the various operating systems that are out there.
Resolution
This is a use at your own risk, it works in most instances when set up correctly but if for some reason it does not, it is an unsupported application.