Monthly temporary (demo/evaluation) license files for Vista 5

Issue

During some circumstances, an additional license may be needed for testing/evaluation/demo purposes. 

Product Line

TAC Vista

Environment

TAC Vista 5

Cause

During some circumstances, an additional license may be needed for testing/evaluation/demo purposes. PSS is creating demo license files with a monthly validity.

Resolution

Monthly demo license files are made by the Malmö PSS team, and may be requested from PSS. The "TS_OK" demo file is used for "Remote Desktop" applications, giving access equivalent to the demo file available for download from the The Exchange Download Center, usually valid until the end of the month. Additionally, a OPC Server license file with the same validity is also available by request.

 

More information can be found in Lessons Learned Article #15931.