Issue
Continuum application fails to start with error 1001 could not load file or assembly Sorttbls.nlp
Environment
CyberStation
Cause
.Net corruption.
Resolution
Uninstall and re-install .net
May have to re-format the hard drive and re-install windows if problem is not fixed by the above.