Replacement of TAC VZ*9 series valves with the Schneider Electric VZ*19* series.

Issue

Cannot order the VZ*9 valves, its no longer available. 

Product Line

Field Devices

Environment

VZ*9

VZ*19E

VZ*19*

VZ*19C

MZ20

Cause

A new line of VZ valves is now available.

Resolution

The old VZ series valves have been replaced with a new. The old (VZ*9) is replaced by the VZ*19* (Either to VZ*19E (Flat face) or VZ*19C (Compression).

The MZ20 actuator range can still be used with the new valve range.

For more information and details, please see  the related data sheets. VZ*9 Valves, VZ*19* Valves, MZ20A Actuators and MZ20B Actuators.