Issue
Generating or importing one XBuilder project into another directly from Vista takes very long time
Environment
TAC Vista
TAC XBuilder
Cause
In v5.1.7, a new feature was introduced that made it possible to import one XBuilder project into another directly from Vista instead of from a file.
TAC XBuilder will by default do a project reference check to determine if the project is included in any other TAC XBuilder projects in the TAC Vista database. If it is included in any other project, the user will be notified in the TAC XBuilder output pane.
The reference check will increase the time it takes for TAC XBuilder to generate the project; depending on the amount of TAC Xenta Servers that exist in the TAC Vista database.
Resolution
It is possible to disable this automatic check in the TAC XBuilder project settings.
- From the menubar click Project and then select Settings...
- In the Settings dialog box uncheck the box that says Check project references in TAC Vista database.