Essex Pin Pad Reader programming

Issue

Essex Pin Pad Reader Programming in I/Net Seven

Product Line

TAC I/NET

Environment

Any Windows OS Version and I/Net Seven Version

Cause

I need to program an Essex Pin Pad reader in I/Net Seven

Resolution

Here is the link to programming the Essex Pin Pad Reader

Essex Pin Pad requires the site is not using Large Numbers

The Essex Pin Pad is for site which wish to use Pin only for entry. Not Pox Card + Pin or Prox only. For information on a Prox card access which includes Pin Pad, check LL article 7491. For a higher security Pin Only option comparable to the Essex, check LL article 7474.