Crystal Reports with I/NET 2.41 and higher

Issue

  • Crystal Reports with I/NET 2.41and higher
  • Design tab is no longer available (missing) within SevenReports.
  • Can no longer edit Crystal (Seven) Reports

Product Line

TAC I/NET

Environment

SevenReports (Crystal Reports) with I/NET 2.41 and higher

Cause

 I/NET will no longer have the "Crystal Reports" Modify and Design license after May 2012. So After 2.41 you will have to buy a separate CD for this function.

Upgrades are not affected by this change. Any SAP Crystal Reports licenses in use at existing installations will still be active after an upgrade.

Resolution

It will no longer be supplied on the I/Net CD. Now you can still View and Print the "Canned" reports, as always. You just cannot modify a "Canned" report or design a "New" report, unless you buy the new CD from Customer Service. Please note, this removal of the Crystal report function will start with I/Net Seven rev 2.41A and beyond.

In order to receive the Crystal Reports application files and license certificate, the SEVEN-REPORTS-RDC part will need to be ordered in addition to the standard I/NET SEVEN software part for each workstation requiring SAP Crystal Reports.

Upgrades (from I/NET Seven Version 2.21 and above) are not affected by this change. Any SAP Crystal Reports licenses in use at existing installations will still be active after an upgrade, as long as you perform an upgrade of the existing I/NET installation.  If you perform a clean install, so you have uninstalled the previous version of I/NET, you will lose this licensing.   Refer to Articles #13133 and #13920 for additional information when upgrading and installing this software.