Issue
After the rehost process, is it possible to use both the old and new licenses (PCs) at the same time?
Environment
TAC Vista 5
Cause
After rehosting a license, nothing prevents you from using both the original and new license file at the same time, since there is no feedback from the system that synchronizes the usage of licenses from the same Entitlement.
Resolution
It is strictly against the license agreement, and should not be used at any time. If a temporary license is required, use the existing demo license files or contact PSS for other temporary solution.