Backing up an OnSite™ building control system.

Issue

How do I backup an OnSite™ building control system once it has been configured.

Product Line

Other

Environment

OnSite

Cause

Need to backup an OnSite building control system in case there is a controller failure.

Resolution

The OnSite™ building control system is an embedded software building control system.  Configuration changes can only be backed up to the controllers non-volatile memory.  It is therefore not possible to create an offsite backup for archiving purposes.