Issue
The customer have some rooms with consumption logs. The customer wants to easily select from and to date, and then be presented with the total consumption in this period. Is this possible in Vista?
Environment
TAC Vista 5.1.7
Cause
You can't do any programming in any objects in Vista(except java script) which you need here. There is no standard object in Vista doing what the customer want.
Resolution
It would be possible to do using a report but then the customer need to create a new report where the trendlog and the input dates is specified every time he need the energy consumption for a certain period.
This is not really what the customer requests so no this is not possible in Vista today.