Field Devices - General configuration of the DC1100 / DC1400 Optimiser Compensator.

Issue

General configuration for these controllers.

Product Line

Field Devices

Environment

Drayton

DC1100

Satchwell

DC1400

Cause

Access to the documentation unavailable and uncertain of the correct configuration.

Resolution

The available controller configurations are all shown in the controller data sheets, please select the required data sheet below.

To review the Drayton DC1100 general data sheet, please click HERE.

To review the Drayton DC1100 "A" data sheet, please click HERE.

To review the Satchwell DC1400 general data sheet, please click HERE.

To review the Satchwell DC1400 "A" data sheet, please click HERE.

For a general overview of the DC1100/DC1400, please click HERE.