Issue
TGML bindings and links are missing and can not be modified.
Environment
Vista 5.1.6
Non-English Windows OS
Cause
The Vista database was created with non-English regional settings and then these settings were changed to US/English. This means that the special regional characters are not recognised in the Vista database.
Resolution
Change the regional settings back to the original settings used to create the Vista database.