Issue
When adding multiple cards to a user where does the number go.
Environment
All versions of I/Net Seven
Cause
When adding multiple cards to a user, depending on which format is being used, the adjacent field is automatically updated.
Resolution
When adding multiple cards to an individual, depending on which format is being used it automatically put the adjacent number in that field.
1. For big card numbers or HEX numbers, those have to be entered in the HEX field and would automatically populate the decimal field.
2. For card number equals individuals, the card number must be entered in the decimal field which will automatically populate the HEX field.