Issue
Making changes to I/O Server with out logging into I/Net or I/Net Configuration
Environment
All versions of I/Net Seven prior to 2.40
Cause
Without login on to I/Net or the Configuration Editor, changes can be made to the system and accepted.
Resolution
When I/Net is launched it authenticates the user thus allowing the changes, however, if the user does not log on, the buttons that require this authentication are all grayed out., So it may look like changes can be made but notice that the OK button does not become available, so no changes will be saved in version 2.40 and above.