Issue
Can the DHCP protocol be implemented on a Niagara R2 UNC-410 controller?
Environment
Niagara R2, UNC-410
Cause
IP Protocol
Resolution
Yes, UNC-410 can use the DHCP Protocol to assign an IP address. Static IP addresses provide the most reliable connectivity between Niagara hosts. It’s recommended that static IP be used over DHCP whenever possible.
Reference “Niagara Networking & Connectivity Guide” for information.