Issue
Valves V354 and V355 requires a specific type of actuator.
Environment
V354 (7315425000)
V355 (7315529000)
M52L (8522320000)
EM52L (8522221000)
EM52L-4 (8522210000)
MC52A (8532221010)
Cause
Due to the design of the V354 and V355 valves, a specific type of actuator is necessary.
Resolution
MC52A, part no. 8532221010, is designed for use as a replacement actuator. It is delivered together with an adapter to fit the V354 valve.