Enterprise Network Server Modbus licensing

Issue

Does the part number, ENS-MOD license the Enterprise Network Server for both Modbus TCP master and slave functions?

Product Line

TAC I/A Series

Environment

I/A Series G3 Enterprise Network Server

Cause

The Enterprise Network Server needs to function as a Modbus master or slave device.  ENS-MOD only licenses the Enterprise Network Server to function as a Modbus master device. It does not license it to operate as a Modbus slave device.

Resolution

ENS-MOD only licenses the Enterprise Network Server to function as a Modbus TCP master (client) device. As of 2013, the ENS can also be licensed as a Modbus TCP Server (slave) using the part number ENS-MOD-SL.