Issue
When upgrading from SX8000 to Cyberstation 1.93, with over 600 reports for SX8000 that need to be upgraded to Cyberstation.
Environment
Cyberstation LAN or StandAlone
Cause
A site has been running SX8000 and is upgrading to Cyberstation 1.93. There are over 600 reports that the customer wants upgraded to Cyberstation.
Resolution
There is no auto-conversion program that will upgrade the reports from SX8000 to Cyberstation. Keywords will be an issue. There are over 600 reports that must be upgraded manually. There is no automatic upgrade for reports.